With targeted use of anti-foam agents enabled by Heartbeat Technology
Industrial wastewater arising from the production of special chemicals and agrochemicals as well as dyes is pretreated separately before entering the ARA Rhein biological industrial WWTP. During the pretreatment process, foam is generated sporadically. Thanks to the new Heartbeat Technology, anti-foam agent can be administered in a targeted and efficient manner, thereby unlocking significant savings potential.
How to save money with foam detection - Video
Benefits of Heartbeat Technology
Detection of foam or buildup
Reduced maintenance
Easy commissioning thanks to guided and interactive commissioning wizard
Features ranging from the generation of verification protocols at the push of a button to the documentation of device testsn
Reduced operating costs
"Targeted use of anti-foam agent can save money - and protect the environment."
Herr Stefan Graser, Wastewater pretreatment foreman
Infrapark Baselland AG
Customer requirements
The industrial wastewater is pretreated at the AVORA before being sent to the biological industrial WWTP. Due to the process involved, extreme levels of foam formation can occur in the 16 m high oxidation reactor. Not only does foam reduce the usable reactor volume and therefore the throughput, but in extreme cases it forces its way into the exhaust system. Anti-foam agent was previously released regularly into the process. This meant that the consumption of anti-foam agent was relatively high.
The Endress+Hauser solution
The Micropilot level radar measures the level in the tank and, thanks to the new Heartbeat Technology, is able to detect the formation of foam on the surface. This ensures that the release of anti-foam agent is initiated in a targeted manner and foam formation stopped. In addition, the AVORA facility at Infrapark uses the Cerabar pressure transmitter for hydrostatic level measurement. This means that in addition to detecting foam, the foam height can also be determined.
La tecnologia Heartbeat dà vita ai dispositivi: fornisce la diagnostica, verifica le prestazioni ed esegue il monitoraggio di tutti i dati di processo per la manutenzione predittiva e l'ottimizzazione del processo.
Prodotti semplici
Selezione, installazione e messa in funzione semplice
Infrapark® Baselland in Schweizerhalle is the ideal location for industrial companies, in particular those in the chemical and life sciences sectors that are involved in research, development or production. Situated in the trinational region of Basel, Infrapark offers a comprehensive range of services and an excellently developed campus of 32 hectares. The “AVORA” wastewater pretreatment facility is an important building block in Infrapark Baselland’s wastewater concept.
Diamo valore alla tua privacy
Utilizziamo i cookie per migliorare la tua esperienza di navigazione, raccogliere dati statistici per ottimizzare la funzionalità del sito e fornire contenuti o annunci pubblicitari personalizzati.
Selezionando "Accetta tutti", ci autorizzi a utilizzare i cookie.
Per maggiori dettagli, consulta la nostra Politica sui cookie .