Spotlight on water quality
Cloud-based system for groundwater monitoring
“Wasserwerk Reinach und Umgebung” (water plant of Reinach and surrounding areas) is successfully using the Netilion Smart System to monitor river levels and key water quality parameters. The measured values can be monitored via smartphone and a distributed control system.
![Reservoir belonging to Wasserwerk Reinach und Umgebung Reservoir belonging to Wasserwerk Reinach und Umgebung](/__image/a/9550481/k/c69e7f64f1c51426cfe4f6d426f4889fec9dc4de/ar/2-1/w/1024/t/jpg/b/ffffff/fn/WWR-D-21-f204b65a2d58aa9g43dc706f3f3bfa3b.jpg)
Vorteile
-
Visualization of recorded measured values in the Netilion ecosystem via web application
-
Entry of up to four limit values per measured variable; alarm signaling via e-mail
-
Fast access to technical documentation
-
Compact analysis panel with flow monitoring
The challenge
e In addition to the water level of the Birs River, measurement of the following raw water parameters is required at one of the groundwater pumping stations: conductivity, pH, turbidity, ORP, oxygen and temperature. These measured values must be routed to the distributed control system and transmitted to a data cloud for remote monitoring via smartphone.
Solution
Thanks to the Netilion Smart System, the river level and the quality parameters of the transported raw water are continuously recorded in a groundwater pumping station. The operational safety engineer and his staff can access the measured data at their PC workstation and on their smartphones via IIoT Netilion. The limit values configured for the measured variables are continuously monitored. The system also provides detailed information on the sensors and maintains the technical documentation.