Essayez la recherche par mots-clés, réf. de commande / code produit ou numéro de série, p. ex. "CM442" ou "Information technique"
Entrez au moins 2 caractères pour démarrer la recherche.
  • Historique
Wastewater Monitoring

Wastewater monitoring

On-site PCR based testing for the Water & Wastewater industry

Simplify your wastewater monitoring with a system that automates the complete workflow from sample to answer.

Wastewater treatment plant ©Endress+Hauser

Proudly overseeing what enters and leaves our wastewater plant…

Water monitoring ©Endress+Hauser

... and monitoring risks for public health.

Objective

Wastewater monitoring is crucial for evaluating public health as it gives a factual outlook without bias. By analyzing the inflowing wastewater, we can detect early indicators of outbreaks.

Equally important is analyzing the outflow to ensure treated water meets safety standards. This confirms that harmful contaminants have been removed, protecting both public health and the environment.

What do we offer?

On-site PCR analyses for:

Inflowing water

  • Discovering the (re)emergence of a health risk

  • Detecting trends and "hot spots"

Water reuse

  • Testing water for contamination before it is reused

  • Ensuring product safety

How does it help wastewater monitoring?

Inflowing water

By identifying rising levels of pathogens, we can detect potential outbreaks early on. Health authorities can take swift action to mitigate risks, such as implementing targeted health measures or informing the public.

Water reuse

Water reuse is an important strategy to address water scarcity. By ensuring it is safe to use, fields, for instance, can have a new water source without affecting product safety.

How does it work?

The Endress+Hauser BioSense Analysis System uses the universal Device BAB00 and special application-specific Kits to automate the entire laboratory process from sample to result.

Find out more here!

Kits for wastewater monitoring:

SARS-CoV-2 Kit

  • Test for monitoring wastewater (inflowing water)

  • Quantification of the SARS-CoV-2 virus

Extensions of the SARS-CoV-2 Kit

  • Swab test for the random sample testing of surfaces

  • Extension of the quality parameters to cover RSV virus and influenza virus

More detailed information and the option to request a quotation have been added to the market sites in which the products are available (DE, AT, CH).

Avantages

  • Simple – the user-friendly system streamlines wastewater monitoring, allowing operators to quickly check for contaminants without needing specialized personnel or laboratory equipment.

  • Fast – state-of-the-art microfluidic automation delivers rapid results, accelerating decision-making to ensure clean wastewater and a safe population.

  • On-site – the compact design of the system makes it possible to perform PCR directly on-site, keeping the entire control process within the facility.

Vous avez des questions ? Nous avons les réponses

Veuillez remplir le formulaire et nous vous contacterons dans les plus brefs délais.

*Obligatoire