Continuous data recording enables targeted optimization
Omlin Energiesysteme AG provides innovative and individually tailored solutions to its customers. An intelligent monitoring system is part of any smart energy system comprising various heating components. The monitoring system records process values correctly and clearly presents them on a display.
Advantages
Flexible and high-performance system to record measured data and calculated values continuously and reliably.
Conventional interfaces, supports a large number of common communication protocols.
Stored data can be read on a laptop or from a USB stick
Remote access to data
"The Memograph M Data Manager can be used to monitor energy systems permanently and optimize them continuously. This guarantees that systems operate transparently and on a sustainable basis.”
Mister Martin Omlin, Managing director
Omlin Energiesysteme AG
Customer requirements
Omlin Energiesysteme AG's innovative heating systems consist of various heating components. To achieve a high level of energy efficiency within the overall system, it is essential to match individual components perfectly. In order to monitor, analyze and optimize the individual processes as well as the overall process, Omlin Energiesysteme requires a measuring and diagnostic system to record and save measured data continuously and to enable the data to be analyzed and displayed locally.
The solution
Omlin chose the Memograph M RSG45 Data Manager as the central system component of the measuring and diagnostic system. The acquired process values are clearly presented on the Data Manager display and reliably recorded. At the same time, the CO2 reductions are calculated based on the recorded measured values.
Omlin Energiesysteme AG, Birsfelden, Switzerland, is an experienced specialist in state-of-the-art heating systems and has a skilled workforce of 14 involved in the planning, implementation and administration of their systems.